Industry Online Support
Technical Forum
12/11/2013 11:46 AM | |
Joined: 10/27/2009 Last visit: 3/15/2024 Posts: 455 Rating:
|
I have seen cycles programmed in the style of the first example but it is not clear what order the parameters need to be given inside the parentheses for each of the measuring cycles. Theprogramming in the requestedstyle: CYCLExyz(Par1, Par2, Par3....) is not available in all SW-versions. The best way to find out: Open a CYCLExyz and check the first line: If the cycle name with a lot of parameters in the brackets will be displayed - the "new" version of programming is available (basically: available from SW4.4 in 840Dsl). The documentationshows how to programm ithe "new" style (Chapter 3). |
hope that helps |
|
12/11/2013 11:53 AM | |
Posts: 11 Rating:
|
Thank you. That does help. I'll have a look at the programs we have on machine. Thanks again. JonS
|
Follow us on