10/24/2014 6:40 PM | |
Joined: 8/2/2011 Last visit: 10/9/2022 Posts: 12 Rating: (0) |
Hello Huggy_d1, thanks for interesting on this threat. I want make application that will have one stepper motor and shaft. Let's take that shaft is long about 500mm. In program i want make scale like this: When bucket on shaft is in position 0mm then in bucket is 0kg, and when bucket is in position 500mm then in bucket is 2kg. I have looking for NEMA stepper motors (http://www.ebay.com/itm/1Pcs-Nema17-Stepper-Motor-DIY-CNC-Router-Mill-Robot-Reprap-Makerbot-Arduino-BDRG-/301354730180?pt=LH_DefaultDomain_0&hash=item462a2442c4), like motors in CNC router applications. I don't want that Siemens PLC control some others controller for stepper motor, I want Siemens module that is compatible with Siemens PLC on same RACK which can be programmed to control stepper motor like in link . So, which is that module
---------------------------- New subject after splitting from SM338 TIA Portal |
Last edited by: Min_Moderator at: 10/27/2014 10:31 AMSplitted |
|
10/28/2014 4:48 PM | |
Posts: 1058 Rating: (93) |
Hello A.P.86, take a look here: Positioning Module IP 247 for Stepper Motors IP 267 Stepper Motor Controller FM 353 Stepper Drive Positioning Module and maybe this one: SIMATIC FM 357-2 Multi-Axis Module for Servo and Stepper Drives regards |
Follow us on