5/16/2007 2:19 PM | |
Posts: 4 Rating: (0) |
Siemens server refresrate = 100 MS In the attachment you can find an acces database in wich I've logged the values. I have done this in 3 ways: 1: From 16-5-2007 13:55:27 to 16-5-2007 13:55:43 // Siemens OPC Server, client refreshrate 100 MS 2: From 16-5-2007 13:55:44 to 16-5-2007 13:56:25 // Siemens OPC Server, forced polling @ about 60 Hz (maximum speed of my application) 3 From 16-5-2007 13:57:45 to 16-5-2007 13:57:54 // Different OPC server downloaded @ http://www.download.com/OPC-Server-for-Siemens/3000-2076_4-10278341.html This latest measurement proofs that my client can poll faster than1Hz. This server is polling @ about 12 Hz(not even close my applications fastest speed but acceptable) For measurement 1 and 2i have looked with OPC scout and could see the server refreshing every 100ms. WithKepware opc quick client I could see the variable refresh @ about 3 - 5 Hz Attachmentdb1.zip (136 Downloads) |
5/16/2007 3:18 PM | |
Posts: 4 Rating: (0) |
Hereby the server LOG AttachmentIVarOPC.zip (151 Downloads) |
5/17/2007 5:32 PM | |
Posts: 324 Rating: (30) |
Hi Obeleh, I would contact Customer Support, they have specialists to analyse this.... I am sure you will get this solved there. |
10/19/2017 10:47 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (174) |
New question published by junaidstar is split to a separate thread with the subject OPC XML SOAP Error. Best regards |
Follow us on