Industry Online Support
Technical Forum
2/15/2011 2:11 PM | |
Joined: 1/1/2008 Last visit: 7/3/2022 Posts: 35 Rating:
|
Hi DEEP, Actually I had to explain existing system. Now here is the explanations: 1) System is to move torch car to cut steel slab in continious casting machine. 2) Motor is a special motor including two motors. One AC motor and one DC motor. AC motor is single speed which move the torch car to the edge of slab, then DC motor (variable speed) will take care of the rest for cutting slab. I have attached the spec of the motor (please take a look at page 6 of the attached file). The controller is a YASKAWA Servopack. I also have attached the connection diagram from servopack to motor. Regards, AttachmentKAE-C240-0H1.pdf (683 Downloads) |
2/15/2011 2:19 PM | |
Joined: 1/1/2008 Last visit: 7/3/2022 Posts: 35 Rating:
|
Here is the connection diagram. |
Follow us on