12/14/2024 12:38 AM | |
Joined: 11/29/2024 Last visit: 12/16/2024 Posts: 1 Rating:
|
Hi, everyone here. I want current control in SIEMOVERT VC SIEMOVERT VC is control to PMG and Generator Excitation system in low power generator plant. I need to test of Generator voltage Step response (2% AVR Step response). Only will control to OPS1 Fail connected SIEMOVERT VC to drive monitor(masterdrive vc 3.03) in manuals, PC not found uss CB addr. in P060 = 7 and defult addr. = 0 (serial port RS232 - cross). and had not setting file. (*.ppp or *.cnl) Want to setting file save and download Device to PC. I want to find model diagram this parameter. I saw parameter Isq(act)[r281] in Current Control sheet. but, not was selected parameter value to P button(OPS1). can I control for SIEMOVER VC final output current in parameter ? SIEMOVERT VC Model : 6SE7021-8EB61-Z = K11+L20 |
We are working on a new user interface with better overview and more relevance.
Follow us on