12/7/2020 4:42 PM | |
Joined: 3/14/2008 Last visit: 9/27/2024 Posts: 2098 Rating: (938)
|
Hi, Generating batch types mean that the configured types in the projects are generated for the Batch project. This occur for:
For example, operation/phase types are generated from the SFC types classified as EPH or EOP. If changes have been made to an SFC type, batch instance or tag collect blocks, the Generate function must be executed again. Propagate function is to make sure that all types are distributed to the individual projects inside the multiproject. Merge will compile all batch instances in the project Transfer OS messages will transfer BATCH specific messages to the OS and afterwards downloading will download all data to the Batch project.
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
Follow us on