5/25/2015 9:21 PM | |
Joined: 3/28/2015 Last visit: 9/23/2023 Posts: 711 Rating:
|
Hello, Kindly have a look at these point: 1-How do you backup/restore with a Comfort Panel?It is not possible to open and process the backup file with WinCC (TIA Portal). The file can only be downloaded to the original or another panel of the same type with a restore procedure. 2-Modify the HMI Program: You should have the original program to be able to edit it . 3-Download the HMI Program: How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet? |
Eng.Mohamed Ibrahim |
|
Follow us on