9/23/2021 6:39 PM | |||||||||||||||||
Posts: 257 Rating:
|
Hello SIOS-Forum-Community, In discussions with customers, the question often arises as to the benefits of SIMATIC Logon and how it is licensed. Benefit With SIMATIC Logon it is possible to realise a central user administration. The central configuration of all access authorisations of a distributed system avoids unnecessary travel times. The cumbersome multiple configuration of each individual station on site is no longer necessary. Accordingly, users can easily be configured centrally. All access data is valid for the entire system on every connected station. Additional access data on local subsystems are no longer necessary. Licensing The PC on which the central user administration is realised must have the corresponding licences.
Note
|
||||||||||||||||
Follow us on