Industry Online Support
Technical Forum
6/9/2011 9:55 AM | |
Posts: 41 Rating: (4) |
Hello THOS. PCS 7 V7.x is not compatible to Windows server 2008! You have to wait for version PCS 7 V8 or use Windows server 2003. PCS 7 compatibility lists: http://support.automation.siemens.com/WW/view/en/2334224 greetings |
6/9/2011 2:31 PM | |
Joined: 1/17/2006 Last visit: 4/16/2024 Posts: 800 Rating: (63) |
Butan Active directory 2008must work. I asume PCS7 is not installed on the DC? |
6/9/2011 8:30 PM | |
Joined: 8/7/2007 Last visit: 12/14/2023 Posts: 4 Rating: (0) |
That's right, PCS7 is indeed installed on a 2003 server.Only the DCis a 2008R2 machine. |
6/9/2011 11:42 PM | |
Posts: 212 Rating: (12) |
hi, First of Simatic Logon compatibilty with 7.0 Sp2 an Sp3 is with some service packs of Simatic Logon PCS7 7.0 SP2 is compatible with SL V1.4 SP1 HF2 PCS7 7.0 SP3 is compatible with SL V1.4 SP3 for login related issue with DC please find info on http://support.automation.siemens.com/WW/view/en/45057192 |