9/12/2022 4:34 AM | |
Joined: 6/23/2022 Last visit: 3/2/2023 Posts: 12 Rating: (0) |
Hello Prof. Frink Thanks for pointing it out. In the Configuration with the new firmware: of the link you provided, I followed the link of ID>17581199 on how to download and install the HSP, and did as the guide said, but I ended up back to the HSP download page Wizard had shared already. It seems that the link Wizard shared, should have and is supposed to fix the problem, but it does not... I also tried seaching the HSP 186, but nothing usefull comes up on the browser... Regards, J.Noguchi |
Last edited by: Jen_Moderator at: 09/12/2022 05:55:19Link optimized. _ |
|
9/22/2022 2:39 PM | |
Joined: 6/23/2022 Last visit: 3/2/2023 Posts: 12 Rating: (0) |
Hi Wizard, Thanks for still making yourself available for this topic. Even after using the HSPS package and updating the HW catalog by selecting all and install all button, CPU still not available, same behaviour as before, I open the project and cannot see program blocks etc. The hardware catalog still the same, there is the folder for the CPU of the project I am trying to open, but it is empty. The question mark I saw is in the HSPS package I downloaded, when manually searching through the files I cold see the CPU I need, but as Prof. Frink mentioned, it is probably just a place holder for other CPUs that use the same firmware. The Drive ES I installed is v5.6 + SP1. Btw when trying to update only the CPU I need, I found out that the HW catalog updater ignores all HSP that has already been supplied within the STEP7, which means I have the file to solve the problem but HW catalog updater wont let me install it as you can see in the attachment. I am guessing the easiest way to solve this is reinstalling STEP7, but I am still looking for a safe way to do that without losing the license key, to be fair I dont even know if this is a valid concern... Best regards, J.Noguchi AttachmentSTEP7 HW catalog update problem.zip (386 Downloads) |
_ |
|