9/6/2022 6:15 AM | |
Joined: 6/23/2022 Last visit: 3/2/2023 Posts: 12 Rating: (0) |
Hello, I have a project that when opened on my Simatic Manager (Step7 V5.6+SP2+HF9), it does not show the CPU or the program blocks. I can open the Hardware config, but then an error pop up [No changes can be made in this station.] and when I click ok, the CPU from the hardware config disappear. I have installed Drive ES lately, could it be a conflict? I have other projects opening without problem btw. Strange thing is on the Step7(Same version but without drive ES) of my coworkers it opens without a problem. Thanks, J.Noguchi AttachmentNew Document.pdf (401 Downloads) |
_ |
|
9/6/2022 6:56 AM | |
Joined: 7/2/2015 Last visit: 4/30/2024 Posts: 96 Rating: (23) |
Hello J.Noguchi, First of all is it an original project or is it a backup from the PLC? And also You can try to do a new project and look if the programm shows you the same issue. If it is, it would be a licence problem or a bad installation
|
If this Information really helps, you could use the Rate function |
|
9/6/2022 7:16 AM | |
Joined: 6/23/2022 Last visit: 3/2/2023 Posts: 12 Rating: (0) |
|
Last edited by: J.Noguchi at: 09/06/2022 07:28:34_ |
|
9/6/2022 8:47 AM | |
Joined: 4/24/2006 Last visit: 5/13/2024 Posts: 8640 Rating: (1151) |
Hello, Yes, that is possible Best regards, Wizard |
9/6/2022 12:54 PM | |
Joined: 4/24/2006 Last visit: 5/13/2024 Posts: 8640 Rating: (1151) |
Hi, Here a link for HSP's: Else you should try: STEP 7 V5.6 SP2 / S7-GRAPH V5.6 SP2 / STEP 7 Professional 2017 SR2 Trial Download Best regards, Wizard |
9/9/2022 1:28 AM | |
Joined: 6/23/2022 Last visit: 3/2/2023 Posts: 12 Rating: (0) |
Hello Wizard, I have updated the HSP without luck. I also did some reasearch on its contents and the CPU I need has a question mark (?) in the article number. I dont know what that means but other items that has a question mark, does not load into the catalog. About the Step7 trial, is there any chance I could endup erasing the license I have when intalling it? Best regards, J.Noguchi |
_ |
|
9/10/2022 7:16 AM | |
Joined: 7/5/2013 Last visit: 5/13/2024 Posts: 3083 Rating: (505) |
Hello J.Noguchi, the "?" is just a place holder. According New Firmware Version V2.8 for S7-300 CPU 319(F)-3 PN/DP you need HSP 186 (not 200). Regards, Frink |
Last edited by: Prof. Frink at: 09/10/2022 07:19:01Last edited by: Prof. Frink at: 09/10/2022 07:24:32Pi is exactly three! |
|
Follow us on