4/13/2016 10:41 AM | |
Joined: 6/14/2006 Last visit: 2/20/2025 Posts: 301 Rating:
|
Hi, SIMATIC NET is a summary topic at Siemens regarding anything that is involved in communication. Including network cables, switches, communication cards and so on. This is valid for all communication protocols such as Profibus, Profinet, Ethernet, Modbus, Foundation Fieldbus and others. So there is not one dedicated manual for all of these. Best is you try to get an overview at http://www.siemens.com/simatic-net SIMATIC PDM is a tool for configuration, engineering and diagnostics of field devices. It is independent if the device is connected via Profibus, Profinet, Foundation fieldbus or others. Start here: http://www.siemens.com/simatic-pdm Regards |
This contribution was helpful to
1 thankful Users |
4/14/2016 9:58 AM | |
Posts: 8 Rating:
|
thanks |
Follow us on