9/18/2008 10:50 AM | |
Posts: 3 Rating:
|
Thanks Abdelaal, but then what is the basis license for? |
9/18/2008 2:41 PM | |
Posts: 487 Rating:
|
Hi Basic is for upto Eric |
Last edited by: aikona at: 9/19/2008 10:04 AMoops |
|
9/19/2008 8:23 AM | |
Posts: 3 Rating:
|
No it is not an emergency disk. Order No. on the diskette is 6GK1704-1LW64-3AA0. |
9/19/2008 9:56 AM | |
Joined: 4/24/2006 Last visit: 4/18/2025 Posts: 8956 Rating:
|
Dear Ayora, Please inform us about the License Type both licenses have? Are they both Floating and Unlimited? Or is Basis license a Trial. Best regards, Wizard |
9/19/2008 1:39 PM | |||
Posts: 487 Rating:
|
Now I am totally confused. |
||
9/19/2008 4:55 PM | |
Posts: 76 Rating:
|
Dear WIzard I think you are rigth , the basis won't be unlimited , it's a trial. Regards Abdelaal |
9/22/2008 12:06 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating:
|
Hello, The basis License means you can use Ethernet. The LEAN License means that you can have up to 8 connections. if you install the Powerpack you will have a third license which is enabling the system to use 64 Connections instead of 8. But it's better to read the description in the following FAQ: |
Best regards, |
|
This contribution was helpful to
4 thankful Users |
Follow us on