Industry Online Support
Technical Forum
5/13/2009 12:56 PM | |
Posts: 9 Rating:
|
Hello Everyone, I'm trying the last days to build and configure an OPC server,this is my firstproject that has to do with an OPC server,i'm dealing now with twochalenges: I will describ first the project: I have two PLC'sSLAVE (2x CPU 317-2DP) and one SLAVE(1x CPU 317-2DP),these PLC's are connected each via a CP 343-1 lean(Ethernet) to aSCALANCE(Firewall+Router) module,which is connected to WINCC OPC server. (1) The first challenge: which version of SIMATIC NET NETWORKINGwill be compatible with CPU317,Simatic NCM PC manager5.3 i think issupporting CPU 314 and not 317(i have tried to make a Hardware update---->> no result(see Attachement)) (2) couldanyone send me a manual. how to build an configure step by step aWINCC OPCSERVER. Can somebody help! Thanks AttachmentOPC.pdf (49 Downloads) |
Follow us on