Industry Online Support
Technical Forum
12/18/2009 9:47 PM | |
Joined: 9/19/2009 Last visit: 2/4/2025 Posts: 459 Rating:
|
Hello! I would like to know, if is possible this. I have a old Simatic Panel Pc 670, but this is out service, because do not work anymore the machine. This panel have Windows NT sp5. The reference number is 6AV7-615-0AB22-0CJ0. I want to install to another machine. Can I make a program with Wincc Flexible and transfer to this Pc? I need install Wincc Flexible Runtime to this PC? How I can do it? Thank you. Regards JM |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
12/21/2009 2:36 PM | |
Joined: 5/13/2008 Last visit: 12/18/2019 Posts: 836 Rating:
|
Hi JM, WCF doesn't support Windows NT. I would suggest you, to organize drivers for Windows XP and install this OS. Some of the needed drivers seems to be available for Windows XP already: http://support.automation.siemens.com/WW/view/en/16968472 Hint: Make an image of all partitions, before you start to update your system to WinXP. Make also some notes of all installed hardware-drivers first. |
mfG / Best regards |
|
Follow us on