12/27/2012 12:34 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, S7 Redconnect based on CP1613 is now called Hardnet IE S7 Redconnect See http://support.automation.siemens.com/WW/view/en/60592369 V8.2 runs on Win7 (not on XP) This version supports also S7 connections based on iso-on-tcp (that runs on top of IP) where previous versions supported S7 connections on ISO only (MAC based). See http://support.automation.siemens.com/WW/view/en/63098071(point c) Because it is delivered together with S7-OPC server, I would advise to investigate if Wonderware can be OPC client and check if that combination is suitable for you. |
Best regards |
|
Follow us on