11/10/2021 9:42 PM | |
Posts: 257 Rating:
|
Hello SIOS Forum Community Multifunctional platform CPUs allow the use of programs written in high-level language C/C++ to reuse existing technological know-how. They can be used as PLC cycle-independent application via an API or/and as PLC function block call in the cycle. The necessary engineering package SIMATIC ODK 1500S contains the well-known editor Eclipse. Model-based code generation for Matlab Simulink uses SIMATIC Target S7-1500S. Plug-and-play of the SIMATIC Memory Card ensures the well-known, long-term spare parts compatibility. An overview of each Multifunctional Platform CPU is listed in the screenshot. Further information: S7-1500 Multifunctional Platform CPU Best regards, SIMATIC Internationa Technical Support Hub |
Last edited by: SIMATIC International Technical Support Hub at: 11/10/2021 21:44:12 |
|
This contribution was helpful to
1 thankful Users |
Follow us on