Industry Online Support
Technical Forum
11/20/2012 11:20 AM | |
Joined: 4/23/2010 Last visit: 9/16/2023 Posts: 8042 Rating:
|
Hello, These are not identical cards. 6SN1118-0AA11-0AA1 is for 611A. Please see this link for more information. 6SN1118-0NH01-0AA1 is for 611U for dual axis control card. Please see this link for more information. |
1/12/2015 4:07 PM | |
Joined: 8/28/2012 Last visit: 9/1/2023 Posts: 4 Rating:
|
The6SN1118 0NH01 0AA1dual axis digital controller card is not a direct replacement for the 611-A controller card. However, it can be used with Engineering by configuring it as an Analog card. This will require recommissioning the drive with SimocomU software. In other words, the 611-U drive will be configured to use an analogue setpoint and digital input for the run command. However, it probably will be necessary to change the motor also. For example, the 611-A cards generally use the 1FT5 motors while it may be necessary to use a 1FT6 with the 611-U drive. |
Follow us on