10/26/2019 12:33 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, 6SN1145-1BB00-0EA1 - 80 Kw Infeed module. 6SN1113-1AB01-0BA1 - Pulsed resistor module. 6SN1123-1AA00-0DA1 - 1 axis 80 Amp power LT module. 611A - 611 series analog drives. Setpoint is +/- 10 volt. Can work with Siemens analog & third party controllers. 611D - 611 series digital drive works with drive bus & compatible with 840D PL CNC 611U - 611 series universal drives communicate with PROFIBUS. Can work with Siemens/third party controller. Please refer the manuals for detail information. |
This contribution was helpful to2 thankful Users |