9/8/2023 8:50 PM | |
Joined: 8/31/2023 Last visit: 10/4/2023 Posts: 14 Rating: (0) |
Attachment29L0119666H_mod_elettrico.pdf (543 Downloads) |
9/12/2023 12:05 PM | |
Joined: 8/31/2023 Last visit: 10/4/2023 Posts: 14 Rating: (0) |
Our spindle has no feed back, it is just a high speed induction motor. This is it, https://www.hiteco.net/en_US/products/electrospindles-a.t.c.c8190/serie-powertech-400-10---13-kw.8205/qe-2-9-6-12-63f-nc-cb.100602 I'll perform the tests you suggest and get back to you with the results. What size motor would you consider a "middle size" one? |
Last edited by: ToddZ at: 09/12/2023 12:07:48 |
|
9/13/2023 2:16 AM | |
Joined: 10/17/2007 Last visit: 5/29/2024 Posts: 3992 Rating: (345)
|
try to find same KW of the spindle motor. spindle motor No feedback will be much more easier to set up. when use SIMO COM U select "no encoder
|
If you like my comments please |
|
9/19/2023 9:58 PM | |
Joined: 10/17/2007 Last visit: 5/29/2024 Posts: 3992 Rating: (345)
|
I try to help you, but (maybe Language issue, what is your country language?) but it seems we are always NOT talking on the same page. --I can suggest you, followed 100% my instruction, or let me you don't need my help any more. Here is my suggestion: SIMODRIVE 611U , I told you is a very good drive system in Siemens drive history , I have been used it for about 30 years (until yesterday) I always use it to testing --don' worry for discontinued , there are more tens of thousand items for this system on line markect Now follow my instruction , and call evey device what i call and it is Siemens calling in your 611U system you have Infeed: module 16/21 KW ---6SN1145-1BA01-0BA1 611U control card, resolve feedback--- 6SN1118-0NJ00-0AA2--(no one call it drive,) Power Section -108A--- 6SN1123-1AA00-0LA0 you have SIMO COM U software in Laptop and communication cable Do you know how to make sure infeed modle working good? - folllow me--now, I attached picture from Manual you need prepare wires /jumers or using switch --see the red wires in picture don't connect DC 600V bars to any other module, also disconnect flat cable (low voltage/control signal) only connect 3 AC power input to infeed module, 1st remove all block 63-9,64-9, 48-112-9 (ter.9 is 24VDC from module to outside) keep NS1-NS2 power up --you need see green LED on , NO any red LED on, then you plug in block 63-9,64-9,--you will see green LED off--good, then you plug in 48-112-9 block you hear click (relay working) and yellow LED on, and you must measring DC about 600V on DC bar P600 to M600 make sure infeed module working good , then I will show how to do next steps AttachmentInfeed_jumps.pdf (430 Downloads) |
Last edited by: nulizhang at: 09/19/2023 22:20:31Last edited by: nulizhang at: 09/19/2023 22:56:29If you like my comments please |
|
Follow us on