7/11/2019 11:31 PM | |
Posts: 14 Rating: (3) |
Hello, Despite a lot of effort, I have not been successful getting SIMOSIM to work. I follow all the step and get the Instance running, but I cannot connect to it ("Connect target device") from Scout. Additionally, I cannot view the instance's Webserver, or ping it. Some details: PC: Windows 7 SP1 Scout Standalone V5.2.1 with SIMOSIM V5.2.1 D435-2, X127 IP: 192.168.127.1 SIMOSIM Adapter IP: 192.168.127.141 Attached is a pdf containing many screenshots of my PC and the configuration, as well as the results. If anyone has anything helpful to add, I would be appreciative. Thank you, David PS. For what its worth, I also tried to disable signatures by pressing F8 at startup (as described here), but no success AttachmentSIMOSIM screenshots.pdf (127 Downloads) |
This contribution was helpful to1 thankful Users |
7/12/2019 6:01 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22230 Rating: (2980)
|
Hello, open the properties of the PLC in Scout an set the online access to DEVICE not to S7ONLINE Regards |
7/12/2019 4:53 PM | |
Posts: 14 Rating: (3) |
Oops, my mistake. I think you are referring to screenshot I shouldn't have put in there. (I tried using S7ONLINE when DEVICE didn't work). I just tried it again with DEVICE again and got the same result. The pdf is updated (the image that used to show S7ONLINE now shows DEVICE) Are there any other tricks or settings you can think of? Thank you David AttachmentSIMOSIM screenshots V2.pdf (119 Downloads) |
7/13/2019 7:21 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22230 Rating: (2980)
|
hi, can ou start accessible nodes and show if anything is displayed? Christoph |
Follow us on