1/10/2017 12:10 AM | |
Posts: 305 Rating:
|
does simotion can via drive-cliq connect smc encoder working master encoder ? is config smc axis must config driver first ? |
1/10/2017 1:33 AM | |
Posts: 1529 Rating:
|
1. Yes 2. Yes, configure the External Encoder in Sinamics Integrated first before External Encoder in SIMOTION |
1/10/2017 4:32 AM | |
Posts: 1529 Rating:
|
You need to create your Sinamics Integrated controller first. |
1/10/2017 4:42 AM | |
Posts: 305 Rating:
|
in test ,wo has not S120, can i to use SIMOTION D425 connect SMC ? |
1/10/2017 5:37 AM | |
Joined: 5/12/2006 Last visit: 4/17/2025 Posts: 22620 Rating:
|
YES |
1/10/2017 6:08 AM | |
Posts: 1529 Rating:
|
Yes, should work fine. |
1/10/2017 6:37 AM | |
Posts: 1529 Rating:
|
Looks OK. No need to create a drive or an infeed. Just Encoder. Then you can attach the TO External Encoder from SIMOTION. |
Follow us on