7/14/2017 11:36 PM | |
Joined: 6/29/2012 Last visit: 12/25/2023 Posts: 975 Rating:
|
I have a SimotionD configured as I-device. That I-device is then connected to S7 400 controller. In the I-device configuration there is the 'standard data' and the failsafe data (failsafe proxy is configured). My specific question is : in the picture 'Idevice2' there is the line with the '70I' that is in 'italic' compared to the previous slots of 'standard data'. Why is that slot in 'italic'? Is there something wrong with the configuration because it is in 'italic'? I must say this is from a working configuration, whithout known problems. AttachmentI-device.zip (328 Downloads) |
7/19/2017 8:51 AM | |
Joined: 4/28/2015 Last visit: 6/5/2018 Posts: 4 Rating:
|
Hallo David, there is nothing wrong this is an indication for safety data. Stefan |
Follow us on