3/4/2011 3:38 PM | |
Posts: 344 Rating:
|
In WinCC Flexible as a first step make sure that the connection with the Simotion connection driver is established: Profibus or Profinet. Then the tag can by symbolically selected (select symbol column in WinCC Flex) from the Simotion controller. Included screenshots for both steps. AttachmentWinCCFlex_Simotion.zip (1047 Downloads) |
3/9/2011 5:47 AM | |
Joined: 12/18/2007 Last visit: 3/18/2025 Posts: 24 Rating:
|
Thank you very much |
6/9/2011 7:45 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Which configuration steps have to be taken in SIMOTION SCOUT and WinCC flexible to enable Alarm_S messages and technological alarms to be displayed in WinCC flexible Runtime? Best regards, Hristo Mihalev |
Follow us on