8/13/2022 12:37 AM | |
Joined: 2/16/2021 Last visit: 11/24/2023 Posts: 11 Rating:
|
Hello everybody I'm using simosim with X127 interface to simulate control and I did establish an HMI connection with the same interface x127 (see the fig attached ) Unfortunately, I can not see any data exchange from the HMI WinCC simulation ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/15/2022 09:41:29New subject after splitting |
|
8/16/2022 5:50 AM | |
Joined: 5/12/2006 Last visit: 4/17/2025 Posts: 22620 Rating:
|
and in PG/PC Setting the simosim adapter is assigned to the accesspoint S7ONLINE? |
8/16/2022 7:07 PM | |
Joined: 2/16/2021 Last visit: 11/24/2023 Posts: 11 Rating:
|
Thank you, ChristoPhd It works now! |
This contribution was helpful to
1 thankful Users |
Follow us on