1/9/2017 12:51 PM | |
Joined: 3/14/2016 Last visit: 5/17/2022 Posts: 161 Rating:
|
Just a correction, if the card is 4-20mA then it's 4mA = 0 and 20mA = 27648 Searching on Google for "SM 1232 manual", second result is SM 1232 analog output module specification6s Attached is specifications for the analog modules of 300/400 family in which you can use the values for underflow, underrange, overrange and overflow for each different analog I/O (0-20mA, 4-20mA, +-10V, 0-10V, ... ) AttachmentAnalog Module.pdf (144 Downloads) |
"Engineers like to solve problems. If there are no problems handily available, they will create their own problems." (Scott Adams) |
|
Follow us on