Industry Online Support
Technical Forum
12/13/2022 10:01 AM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1424)
|
As from TIA V18 there is a ready for use object to get the diagnostic status of a S7 controller in WinCC Unified (Toolbox, Controls, System diagnostic control - stethoscope icon). It is really easy to use, it is just a question of drag and drop it to the screen. TIPs:
simple sample (here to be possible to simulate a fault even without a hardware, an access violation for an array could be triggered by the WinCC Unified screen - this type of fault could be observed in the object, selecting the controller and clicking on the diagnostic buffer button) AttachmentProject8_20221212_0829.zip (444 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
Follow us on