6/20/2021 9:25 PM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1419)
|
Hi, As from WinCC Unified V17 it is possible to use GMP (Good Manufacturing Practice) to register sensible operations production changes. It is the special interest to the pharmaceuticals industry, the food and beverage industry. It is possible to record data from three situations:
There is also three type of entries
A detailed information about GMP could be get in the TIA Information system (show help) under “Visualizing process (RT Unified)”, “Options (RT Unified)”, “WinCC Audit (RT Unified)” Configuration steps:
TIPs:
Sample project AttachmentUniGMP_20210620_1619.zip (1217 Downloads) |
Denilson Pegaia |
|
5/9/2023 9:55 PM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1419)
|
Hi As from TIA V18 (up1), it is possible to use a specific control object (AuditViewer) to see audit data on the screen of a WinCC Unified PC System. New snippets are also available to work with GMP. TIPs:
Sample project AttachmentProjectV18up1_20230509_1850.zip (465 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
Follow us on