10/3/2015 6:40 PM | |
Posts: 1 Rating:
|
Mr Pegaia Is it possible to simulate pulses in the HSC 1 input in the PLCSIM v13? I'd like to simulate pulses of an encoder, then I would use frequency function in the CTRL_HSC and convert it to some speed unit. (m/min for example) I want to use clock memory byte to pulse a 10 hz frequency in the HSC 1 Physically HSC_1 is configured to %I0.0 input In the program I need to use %ID1000 (hardware identifier 257) How to pulse in the HSC+input using PLCSIM? Shold I use the Adress: %0.0 ? ID1000 ? ID1003.0 (LSB)? If I can pulse using PLCSIM, i will move the value loaded in "NEW_PERIOD" convert to real an then make the convertion to speed. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/5/2015 1:03:07 PMNew subject after splitting |
|
Follow us on