12/8/2011 10:46 AM | |
Joined: 10/26/2011 Last visit: 3/24/2025 Posts: 762 Rating:
|
Hello IsaacSanchez It is knwon, that PLCSIM has from time to time communication breakdowns. If the PLCSIM communication breaks down, the connection / communication (SWC = secure write command) between the matrix viewer and the matrix breaks also. That could be the reason of the error message. Regards |
SIMATIC PCS 7 - Overview |
|
Follow us on