7/1/2013 9:07 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Hello, you cannot perform 100% error free software Test with Step7 PLC Sim all the time. Please have a look at similar FAQ which describes Limitation/Function not Supported by PLCSIM. Which components are not supported by S7-PLCSIM V5.4 SP4? Hope this helps. |
VANDE MATARAM..... |
|
This contribution was helpful to
2 thankful Users |
7/3/2013 10:29 AM | |
Posts: 559 Rating:
|
This is really helpful. I was also searching for the same type of simulation solution between 2 plcs. Now I got it. Thanks to all
|
7/3/2013 10:39 AM | |
Posts: 559 Rating:
|
I also want to know one thing. Is it possible to communicate simulation software with hardware plc? Means communication between actual plc & plcsim software.
|
7/3/2013 11:08 AM | |
Posts: 559 Rating:
|
Dear Ayman This is the case if I want to simulate communication between 2 plcs & I have only one plc. Then can I use plcsim as 2nd plc?
|
7/3/2013 2:07 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Hello Soultionfinder, I have worked with some similar product called Simba Profibus available in siemens for simulation Purpose in PCS7. In my Project I communicated 4 AS with around six RIO(ET200M) in each AS. it is used to communicate Remote I/O's with S7 PLC using its own dedicated simba pro Software. With the use of that we can have a benifit in Saving of investments for test, commissioning and training systems. The Details information can be found here regarding the same. |
Last edited by: Amit_86 at: 7/3/2013 2:08 PMLast edited by: Amit_86 at: 7/3/2013 2:08 PMVANDE MATARAM..... |
|
This contribution was helpful to
1 thankful Users |
7/4/2013 1:30 PM | |
Joined: 11/8/2011 Last visit: 7/2/2024 Posts: 387 Rating:
|
thanks for all reply i am getting error while simulating Please find the attached file |
Follow us on