10/31/2014 12:36 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating:
|
Hi Zeyad 315-2 PN/DP supports max of 32 instance of S7 connections, which in turn means theoretically 16 PUT and 16 GET instructions can be run simultaneously. But since only 14 S7 connections are configurable out of 16, it means that all 14 connections can run 14 PUT and 14 GET instructions simulatenous using PN port of 315 PN/DP. Have attached the required page of 315-2 PN/DP. AttachmentS7_connections_intergrated_PN.pdf (164 Downloads) |
6/3/2015 12:36 PM | |
Joined: 9/1/2005 Last visit: 3/10/2025 Posts: 4113 Rating:
|
new question published by rstack is split to a seperate thread with the subject Simultaneous GET FB14 (more than 32) Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on