Industry Online Support
Technical Forum
4/29/2019 8:52 AM | |
Joined: 3/23/2010 Last visit: 3/2/2023 Posts: 20 Rating:
|
hello , I want to start sinamics driver G120 C DP via profibus with s7400 plc and profibus coonnection in the TIA portal, is it possible? I used SINA-SPEED block , but I couldn't start to driver. thank you very much for help. you can see some photos.
Attachmentprj.zip (24 Downloads) |
4/29/2019 10:45 AM | |
Joined: 10/11/2006 Last visit: 12/4/2023 Posts: 5716 Rating:
|
Hello, looks like you are using some old blocks and you are not using telegram 1. Check out the DriveLib SIOS entry, where you can find a manual and the latest versions. https://support.industry.siemens.com/cs/ww/en/view/109475044 You can find an application examples for SINA_SPEED using Profinet, but I think the principle is the same. So you can use those to localize the blocking point in your project. https://support.industry.siemens.com/cs/ww/en/view/109485727 https://support.industry.siemens.com/cs/ww/en/view/109747655 |
With best regards, |
|
This contribution was helpful to
1 thankful Users |
Follow us on