2/18/2016 9:35 AM | |
Joined: 10/11/2006 Last visit: 1/22/2025 Posts: 5985 Rating:
|
Hello, use DPV1. The telegrams are described in the manual. Chapter 6.7.3.2 https://support.industry.siemens.com/cs/ww/de/view/104961375 |
With best regards, |
|
2/21/2016 11:58 AM | |
Joined: 1/16/2012 Last visit: 2/12/2025 Posts: 116 Rating:
|
Dear Tech Team, Thank you very much for reply. In simatic manager I select "universal module" and in STARTER I select "Free telegram configuration with BICO". Input to PLC --> 12 words Output from PLC ---> 04 words For input to PLC (Transmit direction) I select the r2089, r63, r68, r2131, r80, r2089, r82 and r2132 to read the analog and digital information from drive. For output from PLC (Receive direction) I select p1070 Cl: main set point to send the speed set point to drive. Kindly guide me, which parameter I need to select for the command (to start the drive), reset and acknowledge the alarms. Best Reagrds, |
Last edited by: Nisar Ahmed at: 2/21/2016 12:03:14 PM |
|
Follow us on