Industry Online Support
Technical Forum
1/16/2012 9:17 PM | |
Posts: 133 Rating:
|
Hello, More clarification of your system and problem would be helpful to provide you with input. Can you provide a single line diagram of your system. If you have two chassis BLM in parallel I would guess you have a 12 pulse configuration fed by a phase shift transformer possibly. Are both your BLM the same MFLB and do you have seperate reactors on them? Was this system previously running or is this a new installation. If the equipment was running troubleshooting tips would be completely different than a new system installation. AttachmentPages from IH1_Par.pdf (96 Downloads) |
Last edited by: Drives_Coach at: 1/16/2012 10:06 PM |
|
Follow us on