8/28/2019 7:32 AM | |
Joined: 4/28/2015 Last visit: 9/20/2022 Posts: 1278 Rating: (299) |
Hi, I highly recommend to use the SINAMICS DCC Winder application: https://support.industry.siemens.com/cs/ww/en/view/38043750 It is ready to use. So you don't need to program the DCC function on your own, you "just" need to parameterize the functionality. What is also included is the dancer control mode with an integrated PI controller for the dancer position. You can use the analogue input of course to read in the actual position 0-10V. Also the diameter calculation is integrated, which is the main part of a winder system. |
Best regards, |
|
8/28/2019 3:59 PM | |
Joined: 1/17/2013 Last visit: 9/25/2024 Posts: 1105 Rating: (6) |
Dear RB1, Thank you very much I will study first. Best Regards, Vorapob |
Best Regards, |
|
Follow us on