1/23/2018 8:29 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello frebutrilangga, What do you mean by below its device rated DC voltage. From your drive MLFB number, its input rated 3 phase AC supply voltage is 575 Volt , 498 A & rated output DC voltage voltage is 600 V, 600 A DC. You can connect this DC drive to 3 phase AC supply 415 Volt but in such case drive's rated ouput DC voltage would be 432.00 V DC & not 600 V DC. HTH. |
This contribution was helpful to
1 thankful Users |
1/24/2018 6:16 AM | |
Posts: 3 Rating:
|
Thanks you so much. ...sent from App |
Follow us on