10/21/2013 10:00 AM | |
Joined: 10/11/2006 Last visit: 5/27/2024 Posts: 5853 Rating: (793)
|
Hello jonymas, there is a winder application available for Sinamics DCM. Please have a look here. |
With best regards, |
|
10/22/2013 7:38 AM | |
Joined: 10/11/2006 Last visit: 5/27/2024 Posts: 5853 Rating: (793)
|
Hello jonymas, you can get this application free of charge from your local Siemens contact. The download link is the same as already posted, but this download is only visible internal. So your local Siemens contact can download it there and forward it. If you don't have a contact, you can find your local contact here. |
With best regards, |
|
11/5/2013 9:43 AM | |
Joined: 10/11/2006 Last visit: 5/27/2024 Posts: 5853 Rating: (793)
|
Hello jonymas, the Sinamics DCC is part of the Starter installation (by using the CFC checkbox) and it must be installed to use the DCC winder application. But if you use the application without change inside the DCC chart itself(just parameterize it in the expert list), you don't need the engineering license. So if you don't want to change functionality of the example or make own DCC charts, you don't need to buy a DCC license. Beside that, the DCC winder is not part of the DCC license package, it is an application example, providing a DCC chart for winder functionality, which can be imported to CU3x0-2 or DCM and compiled without DCC engineering license (means in this case you can only use the provided parameters and function diagrams, but you can not open the charts except using the 14 days trial license). If your local contact is not familar how to get the example project, he should contact us by the email adress shown in our profile for further support. |
With best regards, |
|