1/19/2017 8:34 PM | |
Posts: 2 Rating:
|
I have a customer who wants to use an S7-1200 to control this motor, and is asking for a Siemens drive. It's a brushless synchronous three-phase AC motor. He needs to ramp it from zero to 2500rpm in ~0.4seconds, then slowly ramp it back to zero. It will consume 32kW peak possibly up to 50kW. It's normally used in electric planes/cars/boats but this is a stationary application. http://www.enstroj.si/Electric-products/emrax-228-motorsgen.html Any suggestions? Thanks in advance! |
Last edited by: AutoGen_844985 at: 1/19/2017 8:41:41 PM |
|
Follow us on