2/26/2021 7:41 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello, If only motor speed is to be measure, no critical referencing required & if encoder cable interfacing length is more (more than 100 m), then you can select incremental HTL encoder with 10 to 30 V DC supply. Depending upon mounting requirement you may select syncho flange or clamp flange & select type of connection you need. Please refer attached sheet, which shall help you to order desired encoder. AttachmentRotary encoder data sheet.pdf (135 Downloads) |
This contribution was helpful to
1 thankful Users |
5/12/2021 7:57 AM | |
Joined: 4/3/2017 Last visit: 9/13/2022 Posts: 15 Rating:
|
Dear experts, Finally I have bought encrement rotary encoder. But How can i wire the encoder to x23 terminal. Encoders information link [snip] AttachmentEncoder.zip (128 Downloads) |
Last edited by: Bayarkhuu.B at: 05/12/2021 07:59:14Last edited by: Jen_Moderator at: 05/18/2021 13:06:19Removed link and added file as an attachment. |
|