12/4/2008 2:07 PM | |
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating: (136) |
Hello KENANK, It is possible to connect a G120 directly to the HMI. The best way to try this is by reading this FAQ: http://support.automation.siemens.com/WW/view/de/29522676 (sorry this is in German, but if i want to switch it in enlish i have to asertain that there is a update but the update is only in german. now you have to possibilities: -wait a few days till it is availeble in englisch -or post your direkt questions and i´ll help you) In my Opinion it´s easy to programming. In your WinCC flexible you have to set as connection a S7 300/400 because the panel think that you want to communicate with a S7. Prepare the adress and the right Baudrate. Now the best: The parameters of the G120 are the same in WinCC flexible. You only have to know what parameters you want to see or control. The r-parameter you couldn´t control because you only can read this. For trying this please download the german example and look it up... regards manfred * * * * * Ho Ho Ho |
12/5/2008 8:13 AM | |
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating: (136) |
Hello, that project is made by wincc flexible 2008. what do you need? wcf 2007? |
12/5/2008 2:13 PM | |
Joined: 12/3/2008 Last visit: 1/29/2009 Posts: 12 Rating: (0) |
i have wincc flex 2005. |
12/5/2008 3:21 PM | |
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating: (136) |
Hello... i convert ist in wcf 05...you only could use this with SP1. * * * * * ??? project |
Last edited by: *Manfred* at: 12/5/2008 3:23 PM |
|
12/5/2008 4:12 PM | |
Joined: 12/3/2008 Last visit: 1/29/2009 Posts: 12 Rating: (0) |
i have SP2 |
12/8/2008 7:58 AM | |
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating: (136) |
then you could download sp1 |
12/8/2008 2:02 PM | |
Joined: 12/3/2008 Last visit: 1/29/2009 Posts: 12 Rating: (0) |
yeah i'll do that....... thanks........ |
Follow us on