9/1/2015 3:13 PM | |
Joined: 3/30/2011 Last visit: 2/10/2025 Posts: 737 Rating:
|
Hello I can confirm Jeff post. Also see here (link to mm4 faq). 2 inverter with peer-to-peer communication is best solution. For no high dyinamic performance sometimes I made torque control also with probibus communication beetwen inverters. Regards |
★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ |
|
This contribution was helpful to
1 thankful Users |
9/2/2015 5:41 AM | |
Joined: 11/21/2007 Last visit: 12/23/2024 Posts: 2325 Rating:
|
Hello all Many thanks for your replies. @jeff - Yes, we have provided individual motor overload protection at the output of the drive. As per the FAQ Sensorless vector control is possible if the motors are mechanically coupled. : and NO the application does not require a high dynamic response. please correct me if I am missing something. Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on