5/2/2020 10:09 AM | |
Joined: 3/27/2008 Last visit: 12/4/2023 Posts: 1041 Rating:
|
The attached circuit is using 'strapping', to produce a DC Voltage double that of the AC 230 Volt input. The output is DC at some 640 Volts, connect this to two of the phase terminals of the inverter input, and also set Parameter P210 to its highest Voltage, 480Volts from memory. This will be suitable for low power motors, if the load is too great the supply will collapse. It is possible that a pre charge circuit would be a beneficial modification, not something I put in however. This works for Micromaster and Sinamics drives as demo units, I will leave you to interpret this circuit as safe to use in your application. N.b. The caps are Electrolytic. Tractor AttachmentVoltage conv ckt.ppt (355 Downloads) |
Last edited by: Tractor at: 05/02/2020 10:14:03Last edited by: Tractor at: 05/02/2020 12:18:41Tractor |
|
This contribution was helpful to
1 thankful Users |
5/5/2020 2:24 PM | |
Joined: 8/24/2011 Last visit: 11/28/2023 Posts: 68 Rating:
|
thaks dear friend, i attached the circuit again, so please check the polarity of the capacitors, if it's right AttachmentVoltage conv ckt.ppt (323 Downloads) |
5/5/2020 4:00 PM | |
Joined: 3/27/2008 Last visit: 12/4/2023 Posts: 1041 Rating:
|
Polarity is correct |
Tractor |
|
5/5/2020 5:44 PM | |
Joined: 8/24/2011 Last visit: 11/28/2023 Posts: 68 Rating:
|
thanks for the information Last question. i have here in my lab some capacitors, 470mf x 400 volts. can i use this? |
5/6/2020 9:26 AM | |
Joined: 3/27/2008 Last visit: 12/4/2023 Posts: 1041 Rating:
|
Thanks for the feedback Tractor |
Tractor |
|
Follow us on