1/22/2016 1:35 PM | |
Posts: 3 Rating:
|
Hello all, I have a question concerning the Sinamics link between CU3210-2-DP. I have 4 drives and every time one of them is the master and the rest the slaves. When one is the master, needs to send his actual torque to the slaves for enabling the droop. So the problem is that I would like that when one is the master to send his torque to the rest, but the slaves not to send to the master since the master does not require droop. But there is flexibility of whom is the master. Every drive can be a master or a slave, so I want to activate every time whether one drive will receive or transmit via CBE20 sinamics link. Is this possible? I thought to do it by deactivating the sinamics link to the master via p8837 everytime with the input that defines whether one is a master or not, but that would mean that does not transmit also. Is there anyway to do that, like in the DCM drives? Thanks a lot. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/22/2016 3:29:40 PMNew subject after splitting |
|
1/25/2016 1:31 PM | |
Posts: 3 Rating:
|
Hello Sorry I was taking about CU320-2-DP. Is it possible? |
11/18/2016 7:00 PM | |
Joined: 2/25/2014 Last visit: 1/26/2023 Posts: 61 Rating:
|
https://support.industry.siemens.com/cs/ww/en/view/109477831
OA_Application is possible... Please refer to link site.. |
Follow us on