Industry Online Support
Technical Forum
6/22/2009 11:51 AM | |
Posts: 139 Rating: (25) |
This stumped me tooand I found thatUmencho has already answered this one in the below link /tf/WW/en/Posts/25357 |
6/22/2009 12:09 PM | |
Posts: 26 Rating: (0) |
Hi Anchobi, but I don't know what the CF card is. Does it mean the CP card or is something related to the Drive itself? Thanks a lot |
6/22/2009 12:28 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, CF means compact flash card of the control unit (CU). The easiest way (and 100% sure that you use the right file) is to take necessary gsd from there. You should take this card, and using normal card reader in windows explorer... After just install this file in HW Config. Go in Options - Install new GSD file... Other way is to update your hardware catalog. Deppends what version of Step7 you have. Look at How can you update the hardware catalog without direct Internet access? or with internet connection How do I update the STEP 7 module catalog Hope this will helps. Best regards Hristo Mihalev |
6/23/2009 2:49 AM | |
Posts: 160 Rating: (16) |
Have a look at the following FAQ. This should anwser all your questions. http://support.automation.siemens.com/WW/view/en/27196655 |
6/23/2009 8:05 AM | |
Posts: 26 Rating: (0) |
Thanks for your help guys, I will contact someone from Siemens and I'll have a look at the weblink as well. |
6/18/2014 1:46 PM | |
Posts: 5 Rating: (0) |
please provide Link of GSDML file 6SL 3244-0BB13-1FA0 |