4/25/2013 8:47 AM | |
Posts: 4 Rating: (0) |
It's a induction motor whitout drive-click, so i am making a offline commissioning. The status of p10 is (0) ready. |
4/25/2013 8:48 AM | |
Posts: 4 Rating: (0) |
And I don't use the safety fuctions already. |
4/25/2013 10:18 AM | |
Joined: 10/11/2006 Last visit: 4/18/2024 Posts: 5819 Rating: (787)
|
Hello, With such a message F31131 it could be a problem in the encoder wiring or in the encoder configuration. In this case you could call the hotline for such a topic. http://support.automation.siemens.com/WW/view/en/16605032 |
With best regards, |
|
6/20/2013 11:06 AM | |
Joined: 9/13/2010 Last visit: 3/21/2024 Posts: 30 Rating: (1) |
Hi, Did you resolve your issue?? I'm experiencing the same problem, my encoder is absolute SSI sin/cos. |
1/21/2014 11:37 AM | |
Posts: 340 Rating: (6) |
new question is splittet to I want to control S110 from PC. |
Follow us on