6/15/2010 4:12 PM | |
Posts: 20 Rating: (0) |
Dear all, I'am using an safety plc. I have configured an ethernet network. I have to use profisafe but i don't no how ? Thank you. |
6/15/2010 4:28 PM | |
Joined: 5/12/2006 Last visit: 12/20/2024 Posts: 22482 Rating: (3039)
|
Hello, |
6/16/2010 1:01 PM | |
Posts: 20 Rating: (0) |
dear all, I cannot select profisafe. See screenshot. Thank you. |
6/16/2010 3:58 PM | |
Joined: 5/12/2006 Last visit: 12/20/2024 Posts: 22482 Rating: (3039)
|
Double Click on the Slot 1 ("DO with..:) and open the tab "options" In this Options tab you can select PROFISAFE |
6/16/2010 4:13 PM | |
Posts: 20 Rating: (0) |
I can't select the tab options. See screenshot. |
6/17/2010 6:50 AM | |
Joined: 5/12/2006 Last visit: 12/20/2024 Posts: 22482 Rating: (3039)
|
Hello, which SW-Version you have installed? STARTER? STEP7? Distributed Safety? Regards Christoph |
6/17/2010 8:28 AM | |
Posts: 20 Rating: (0) |
Dear ChristophD, I'am using step 7 V5.4 + SP5. S7 distributed safety V5.4+SP5.I have uploaded the used gsd file. Thank you. Attachment2.6 gsd.zip (370 Downloads) |
Last edited by: elmucho at: 6/17/2010 8:40 AM |
|
6/17/2010 11:50 AM | |
Posts: 20 Rating: (0) |
Dear ChristophD, Do i need starter or drive es basic software ? Thank you. |
6/17/2010 12:09 PM | |
Joined: 5/12/2006 Last visit: 12/20/2024 Posts: 22482 Rating: (3039)
|
Hello, i think STARTER is enough, because you have already installed Step7. Regards Christoph |
Follow us on