5/9/2021 11:43 AM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980)
|
Hi Cu310-2 dp not supported in tia, only the cu3x0-2 pn |
This contribution was helpful to1 thankful Users |
5/10/2021 10:16 AM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980)
|
which Starter Version? |
5/10/2021 11:42 AM | |
Joined: 5/6/2021 Last visit: 3/25/2023 Posts: 9 Rating: (0) |
Drive ES -Starter V:4.2.0.0 |
5/10/2021 11:44 AM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980) |
try it with a newer Version latest version is V5.4 UPD2 |
5/10/2021 12:10 PM | |
Joined: 5/6/2021 Last visit: 3/25/2023 Posts: 9 Rating: (0) |
I installed ِDrive.ES.Basic.v5.5 but the starter 4.2 was installed Please send the link address |
5/10/2021 12:11 PM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980) |
https://support.industry.siemens.com/cs/ww/en/view/26233208 |
5/11/2021 5:44 AM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980) |
this module is available. please check that you use the correct FW Version of cu (V4.7 or above) |
Follow us on