11/15/2019 6:30 AM | |
Joined: 5/12/2006 Last visit: 10/2/2024 Posts: 22388 Rating: (3015)
|
Hello, check the parameters 11x, this are the parameters for Cycle time inside the system. Regards Christoph |
12/10/2019 11:42 AM | |
Joined: 10/16/2018 Last visit: 9/11/2024 Posts: 38 Rating: (0) |
Hello Cristoph, What parameters do you mean by 11x? We have a machine with 22 axis.You can find the configuration at attached file. We receive a drive cliq error at random times.Simotion version is V5.1 and cu version V4.8. The error codes I received are as follows: F30835 Power Unit DCLIQ:Cyclic data transfer error F31835 Encoder DCLIQ:Cyclic data transfer error F30875 Power Unit DCLIQ:Suppl voltage failed(Undervoltage) F30885 CU DCLIQ:Cyclic data transfer error F31885 Encoder 1 DCLIQ:Cyclic data transfer error F30008 Power unit:Sign of life error cyclic data F30820 Power unit DCLİQ:Telegram error F31820 Encoder DCLİQ:Telegram Error F31860 Encoder DCLİQ CU:Telegram Error. I changed the all drive cliq cable and I measured line supply voltage as solution. Line supply voltage seems well . I measured long term with a voltage analyzer. Maybe I can solve the problem by extending the drive cliq cycle time. Could you say 11x parameter mean ? AttachmentConf_and_Faults.zip (134 Downloads) |
5/11/2020 8:12 PM | |
Posts: 1 Rating: (0) |
Hello Mr. İsmet, Have you find a solution for F31885 fault. I have same problem. Thanks |
Follow us on