11/28/2018 8:53 AM | |
Joined: 1/22/2018 Last visit: 7/19/2022 Posts: 2 Rating:
|
Hi experts, We are using CU310-2 PN that has connected SMC30 it topology. On that SMC30, over EXE101(Heidenhain), we have connection with Heidenhain length gauge MT101M. We are receiving A and B signals from length gauge but I am not able to set function in STARTER reset actual value with zero mark. (Lenght gauge has reference mark 10 mm from the top) On this link below: https://support.industry.siemens.com/cs/de/en/view/109477773 It is confirmed that we can reset value XIST_ERW with zero mark. I have set parameter p4652 to [1] Reset with zero mark. When we look at the value XIST_ERW it is not changing and we can't do a reset. On top of that we have encoder error. (Attached photo) Multiple times we checked connection in our system and it is ok. How can I setup my STARTER project so that my Lenght gauge connected to SMC30 resets XIST_ERW when we hit zero mark? Thank you, Dino |
Last edited by: Jen_Moderator at: 11/28/2018 11:34:56 AMOptimized link. |
|
Follow us on